RedChannel Tab plug-in fails to load

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RedChannel Tab plug-in fails to load

606 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by robert.palmer on Wed Feb 22 15:45:36 MST 2012
I'm not sure what the "RedChannel" tab in LPCXpresso is for, but I get the following error when I select this tab:

Could not create the view: Plug-in com.crt.lite.brand was unable to load class com.crt.config.browserview.RedInfoView

Is this something I need to concern myself with?  What is supposed to be shown in this tab?  How do I fix the issue?
0 Kudos
Reply
1 Reply

598 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Wed Feb 22 16:02:46 MST 2012
it is irrelevant. You can ignore the errors.
0 Kudos
Reply