[Red Suite] Using Recorded of LPC-Link

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[Red Suite] Using Recorded of LPC-Link

1,432 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bruno on Tue Oct 02 12:11:24 MST 2012
Hello, people

I retired resistors ( R31, R36, R35, R33, R32) and connected J5 in the Evalution Board. The Red Suite show when recorded programme in LPC2387 the following message:

http://www.netupload.org/visualizar.php?arquivo=bxnab1ojf1vcfgwhbtvm.jpg

http://www.netupload.org/files/bxnab1ojf1vcfgwhbtvm.jpg


Do I need to change some configured of Red Suite 4 or LPC-Link?

I used LPC-Link of LPC1343 Rev A and one board with LPC2387.


Thank you very much
0 Kudos
Reply
7 Replies

1,425 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bruno on Tue Oct 09 12:57:41 MST 2012
This board that I connected in LPC-Link 11U14.


[IMG]http://www.netupload.org/files/2jevm18lflr8zwgkgndb.jpg[/IMG]

[IMG]http://www.netupload.org/files/vs8z15wht88vlpxpzfvt.jpg[/IMG]

Previously, I posted that resistors removed in LPC-Link 11U14
0 Kudos
Reply

1,425 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bruno on Tue Oct 09 12:51:44 MST 2012
First,

I started project with main empty. The chip is selected correct.

See picture.

[IMG]http://www.netupload.org/files/r0esiolgk6mxpd92289g.jpg[/IMG]

So is show this error after compilater of programme.


[IMG]http://www.netupload.org/files/gvhg32xtq4e0c2pow5pm.jpg[/IMG]

Is first time that I recorded LPC2387 with JTAG. I used LPC11U14 for recorded. The code can not recorded in chip.
0 Kudos
Reply

1,425 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Tue Oct 09 12:43:54 MST 2012
Did you ever get access to your 2387 with JTAG?

Which code is running in your 2387?

Did you try to switch your 2387 to ISP before using JTAG?

Did you try to erase your 2387 with FlashMagic before?
0 Kudos
Reply

1,425 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bruno on Tue Oct 09 12:33:48 MST 2012
Hello, Zero

I checked all pins, and doesn't anything wrong in connections.

Do you know that can is wrong? Deleting the part of connections.


I'm confusion, because this doesn't work.

Thank you.

Zero.
0 Kudos
Reply

1,425 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Tue Oct 09 11:55:12 MST 2012
LPC2387 has no SWD, so a working JTAG is necessary for this chip ;)

JTAG and SWD require different connections, see:

http://www.support.code-red-tech.com/CodeRedWiki/HardwareDebugConnections?action=show&redirect=CM3_S...


Quote:

Normally where both modes are supported, Red Suite will default to using SWD mode.

So probably your LPC11U14, LPC1343 and LPC1769 are working with SWD :)
0 Kudos
Reply

1,425 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bruno on Tue Oct 09 09:51:51 MST 2012
But for ARM7 SWD and JTAG are compatible, or not?

I trying whit various board for example: LPC11U14, LPC1343 and LPC1769. And any works in LPC2387.
All conections is right. What can is wrong?
0 Kudos
Reply

1,425 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by OXO on Tue Oct 02 14:50:04 MST 2012
LPC11xx is SWD, not JTAG.

You will find the connections for that on the red suite website, or by searching in this forum.
0 Kudos
Reply