Red State / SCT shadow registers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Red State / SCT shadow registers

819件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tiziano.annoni on Mon Apr 23 08:29:32 MST 2012
Dear all,
is anybody using red state SCT graphical configuration tool?
Does it support shadow registers of SCT peripheral?

Thank you!
Best regards,

Tiziano
0 件の賞賛
返信
1 返信

797件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon Apr 23 17:17:12 MST 2012
The Red State graphical tool allows you to set initial values to be used in match registers in the GUI tool.  It also defines macros in the sct_fsm.h to set values for the reload registers from software.

You can add capture registers in the Output view using the green plus button. These registers can also be accessed through software using the macros generated in the sct_fsm.h file.

Regards,
CodeRedSupport
0 件の賞賛
返信