ROM/RAM usage in MAP file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ROM/RAM usage in MAP file

1,762 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mohsin on Fri Jan 07 03:58:23 MST 2011
Hi All,

          I am using LPC1114. I was wondering how to find the ROM/RAM usage once we do a build. Usually the MAP file shows how much ROM/RAM in % has been used but the MAP file generated for LPC1114 has no such information.

        Regards,
        Mohsin.
0 项奖励
回复
3 回复数

1,582 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Feb 16 12:24:51 MST 2015
You will need to extract this from the information in the map file generated by the linker at build time (typically in the Debug/Release directory). For more information, see:

http://www.lpcware.com/content/faq/lpcxpresso/application-flash-ram-size

You could also take a look at the symbol viewer...
http://www.lpcware.com/content/faq/lpcxpresso/symbol-viewer

Regards,
LPCXpresso Support
0 项奖励
回复

1,582 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by esso on Mon Feb 16 07:35:47 MST 2015
Hello,

Is there any way to get the ROM/RAM usage per function?
Thanks.
0 项奖励
回复

1,582 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Fri Jan 07 09:06:10 MST 2011
The size of your application is reported at the end of the log in the console view when you do a build. For more information, see:

http://knowledgebase.nxp.com/showthread.php?t=522

Regards,
CodeRedSupport
0 项奖励
回复