Question about Magjack

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question about Magjack

1,001件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by serge on Wed Jul 20 01:02:30 MST 2011
Hello all,

Zero I have read your threads about how to connect a magjack to the lpcxpresso boord 1769 but my question is would this one do the job? http://be.farnell.com/stewart-connector/si-61007-f/magjack-rj45-gigabit-w-o-leds/dp/1572193

I have a couple of those within handreach. I have only one problem: where to connect pin 10 of this magjack?

Kind regards,
Serge
0 件の賞賛
返信
2 返答(返信)

991件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by serge on Wed Jul 20 02:57:09 MST 2011
Thanks Zero,

It is a first time that i am going to use an ethernet connection in one of my designs, so i am not really familiar with how to connect things. But i learn fast :D
0 件の賞賛
返信

991件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Jul 20 02:54:24 MST 2011

Quote: Serge
...where to connect pin 10 of this magjack?




VIO (3.3V) :eek::eek:
0 件の賞賛
返信