Project Stopping At run point in Debug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Project Stopping At run point in Debug

1,156件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by anchalia.vivek on Mon Aug 18 10:29:18 MST 2014
Hello Everyone,
I have an issue when I try debugging my project it stops at run point. A message in the debug window shows this

" Writing to the flash ......" But it stops at run point .


Can anyone help.??

What can be the issue it tries and stops at point where I have to press resume and stop in the end.

Thank you,
Vivek

0 件の賞賛
返信
3 返答(返信)

1,148件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Aug 20 02:12:21 MST 2014
As per our previous request, please post you debug log too.

Can you also let us know if you have ever been able to program this board, and if the problem only affects a specific project?

Regards,
LPCXpresso Support
0 件の賞賛
返信

1,148件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by anchalia.vivek on Tue Aug 19 10:50:49 MST 2014
hello,
Thanks for replying

1) The version is LPC 7.3.0 on Windows 7 OS
2) The board is a Assembled Board which has MCU, Ntag, Sensor.
3) Target MCU is LPC812 XSON package
4) Debug probe is LPCExpresso LPC Link 2


Thank You.

0 件の賞賛
返信

1,148件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Aug 18 14:34:25 MST 2014
If you want help, then you'll need to post some more details. For example…

What version of LPCXpresso IDE running on what host OS?
What board?
What target MCU?
What debug probe?

Have you ever successfully debugging with this set up?

Does the problem happen with just one project or all projects?

And please post your full debug log too:

http://www.lpcware.com/content/faq/lpcxpresso/debug-log

Regards,
LPCXpresso Support
0 件の賞賛
返信