Programmer for LPC1114FHI33/302

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Programmer for LPC1114FHI33/302

699 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Dore on Mon Jan 13 01:51:42 MST 2014
Hi,

I have designed my board with LPC1114FHI33 controller.
I have also built my hex & bin file for my sample application.
I would like to program this hex/bin file from a PC programmer application (similar to FlashMagic) to program my board with the hex/bin file through LPCXpresso debugger.
Note: I do not want to use the LPCXpresso IDE for programming, instead I would like to use some PC application similar to Flash Magic and also I cannot use Flash Magic since I didnt make the provision in the board to bring into the ISP mode, so I may not be able to use the FlashMagic.

If you had come across any such situations please let me know.

Best Regards,
Dore
0 项奖励
回复
2 回复数

692 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Dore on Tue Jan 21 07:19:23 MST 2014
The thing here is when the board is empty (without any firmware/secondary or user boot loader loaded into the flash), with this scenario we would like to load the combined firmware file into the flash (We have the boot loader & application code both has been kept into a single bin/hex file).
0 项奖励
回复

692 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Mon Jan 13 04:38:20 MST 2014

Quote: Dore
... cannot use Flash Magic since I didnt make the provision in the board to bring into the ISP mode, so I may not be able to use the FlashMagic...



Then just use software to switch to ISP: 'Reinvoke ISP' (IAP 57) is described in UM...
0 项奖励
回复