Problems with altering counter match value witin the ISR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems with altering counter match value witin the ISR

673 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JSalisbury on Thu May 12 08:26:20 MST 2011
Hi,
I am useing a 16 bit counter to count incoming pulses and trigger interupt on count = match value. I would like to be able to change the match value within the ISR, what is the safe way of doing this.

I have tried the code shown but I do sometimes get errors such as
" Single stepping until exit from function __write,
which has no line number information. when single stepping"

Thanks


/******************************************************************************
** Function name:        reset_timer
**
** Descriptions:        Reset timer
**
** parameters:            timer number: 0 or 1
** Returned value:        None
**
******************************************************************************/
void reset_timer16(uint8_t timer_num)
{
  uint32_t regVal;

  if ( timer_num == 0 )
  {
    regVal = LPC_TMR16B0->TCR;
    regVal |= 0x02;
    LPC_TMR16B0->TCR = regVal;
  }
  else
  {
    regVal = LPC_TMR16B1->TCR;
    regVal |= 0x02;
    LPC_TMR16B1->TCR = regVal;
  }
  return;
}




void TIMER16_1_IRQHandler(void)
{
    /*
     *  adc_data_buff 0=x 1=y 2=Z
     */
    int i;
    int curr_ch;
    uint32_t local_v;

  if ( LPC_TMR16B1->IR & 0x1 )
         {
      SSP_Receive( 1,debug_rx_buff_local, 3 ); //perform read regardless if the data is needed reduce jitter
          switch (counter_control)
          {
          case reset_adc:
        TESTPIN_1_ON;
          SYNC_N_HIGH;
          drdy_count = ADC_BURST_LIM;
          counter_control=adc_drdy_wait;
          MUX_0_LOW;
          MUX_1_LOW;
        LPC_TMR16B1->MR0    = DRDY_LONG ;  // these lines can cause lockup
    reset_timer16 (ADC_COUNTER); // these lines can cause lockup
        LPC_TMR16B1->IR = 1;
          break;
}
return;
}
0 Kudos
Reply
1 Reply

664 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JSalisbury on Mon May 16 01:29:36 MST 2011
Problem solved,
trying to single step DBPRINTF gives strange results.
0 Kudos
Reply