Problems with ADC on demoboard

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems with ADC on demoboard

615件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wama on Mon Dec 12 04:08:43 MST 2011
[FONT=Helv][SIZE=2][FONT=Helv][SIZE=2]Hello,
I'm new in programming with nxp.
For this reason I am trying to program some applications with the LPCXpresso demoboard.
On my board (LPC1200) the mcu LPC1227 is included.

After installing and activating the IDE (v4.1.0) on Windows XP I downloaded the example projects for the LPC1200 series. Now I have some troubles with the ADC project.

For the conversion I tried to use the channels 0,1 and 2. But the result is always the same. Every time I get the value 1023. Even if nothing is connected to the port. I just changed the port configurations to use another port for the conversion.
Until now I just tried to work in debug mode. I read someting about similar problems in the past. But they could fix the problems with an update of the IDE.

It would be great if somebody could help me to find a solution.
Thank you
[/SIZE][/FONT][/SIZE][/FONT]
0 件の賞賛
返信
1 返信

604件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Europe on Thu Dec 15 05:44:39 MST 2011
Hello mawa,

how dit you read the '1023'?

Did you connect an external UART to read the 'printf'?
0 件の賞賛
返信