Problems activating LPCXpresso 6.0.4 Free Edition for OSX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems activating LPCXpresso 6.0.4 Free Edition for OSX

961 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gjw on Fri Oct 11 11:33:52 MST 2013
Hi,

I can't seem to be able to activate my newly downloaded LPCXpresso 6.0.4 (OSX) as a Free edition on a macbook pro. Once I created the serial number and entered the activation code (but before restarting LPCXpresso), it shows

Enter Activation code...
LPCXpresso
License type: FULL
Debug limit: 256k
Activation code: ESJS-BSB3-C1EX-JVER-AXBZ-DQA5-AVKU-D4BQ

When I press OK, i get prompted "LPCXpresso must be restarted. Restart Now?". Once restarted, it comes back with

LPCXpresso (Pro Edition)
License type: UNREGISTERED (Code=4)
Debug limit: 8k
Activation code: not available
To activate a license, please select
Help->Activate LPCXPresso (Free Edition)


Additional info:
- I have a Full version of RedSuite 5 OSX installed (but not running) in parallel. This works fine.
- I have removed and re-installed LPCX 6 multiple times and tried different workspaces. Removed previously used workspaces. I tried again after rebooting and after creating another account on lpcware.com for the activation just to make sure - same thing.

Any advice?

Thanks in advance!

Regards,
guido
0 Kudos
Reply
3 Replies

913 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gjw on Sat Oct 12 02:56:00 MST 2013
Even manually changing permissions to rw for everyone on that directory and all files within didn't help (every time I re-started LPCX, LPCXpresso.acc was re-set to -rw-r--r--, all other files remained writeable to everyone). However, re-installing the app once more & launching via "Open lpcxpresso" link eventually did the trick - not sure why. 

Thanks for your help!
0 Kudos
Reply

913 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Sat Oct 12 00:22:38 MST 2013
The license file are stored in
/Users/Shared/NXPLPCXpresso

Please check the file permissions on that directory and the files within, to make sure that you have write permission.
0 Kudos
Reply

913 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by liaochengyi on Fri Oct 11 23:53:21 MST 2013
Hi,

I am Licensed LPCXpresso (Free Edition) 6.0.2 OK for Mac OS X.
I think it's also OK in 6.0.4.

It will send e-mail to you, open the e-mail, link to website to get the code and sign in...

-----------------------------------------------------------------------------------------

License type: FULL
Debug limit: 256k
Activation code:

A FULL copy of LPCXpresso (Free Edition) may be used for production.

Install path: /Applications/lpcxpresso_6.0.2_151/lpcxpresso/

Product: LPCXpresso
Activation date: N/A
License file: /Users/Shared/NXPLPCXpresso/LPCXpresso.sib
Version: LPCXpresso v6.0.2 [Build 151] [2013-09-18]
Operating system: Mac OS X
VM: Java HotSpot(TM) Client VM (32 bit)
About: {0}
0 Kudos
Reply