Problem with registration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with registration

1,055件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Savelev Andrey on Thu Feb 04 06:04:18 MST 2010
Hello !

Mail server that will send confirmation of registration is not working properly. Any mail server that is configured correctly in terms of security does not accept mail from him.

[SIZE=2]Feb 4 15:29:43 mxcb postfix/smtpd[3457]: 84C1174: reject: RCPT from lpcxpresso.code-red-tech.com[67.222.16.169]: 450 4.7.1 <host.cm0tools.com>: Helo command rejected: Host not found; [/SIZE][U][SIZE=2][COLOR=#0000ff][SIZE=2][COLOR=#0000ff]from=<[email protected]>[/U][/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2] [/SIZE][U][SIZE=2][COLOR=#0000ff][SIZE=2][COLOR=#0000ff]to=<andrey*******@***********.ru>[/U][/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2] proto=ESMTP helo=<host.cm0tools.com>[/SIZE]
[SIZE=2][/SIZE]
[SIZE=2][SIZE=3]While he would not mention his proper name, of him nothing will.
This is a protection against spam-server works. Works as it should.[/SIZE][/SIZE]
[SIZE=2][SIZE=3][/SIZE][/SIZE]
[SIZE=2][SIZE=3]WBR, Andrey[/SIZE][/SIZE]
[SIZE=2][SIZE=3][/SIZE]
[/SIZE]
0 件の賞賛
返信
1 返信

1,012件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Feb 04 07:25:44 MST 2010
Hello,

Thanks for reporting this. We have reconfigured the server so this should no longer be a problem. Please let us know if the problem is not solved.

Thanks
0 件の賞賛
返信