Problem with LPCXpresso 4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem with LPCXpresso 4

802 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by micrio on Wed Jun 29 10:30:30 MST 2011
[SIZE=4]I installed the new version 4. I installed all the examples. When I try to build the adc example I get:[/SIZE]

[LEFT][SIZE=4]make clean [/SIZE]
[SIZE=4]0 [main] us 0 init_cheap: VirtualAlloc pointer is null, Win32 error 487[/SIZE]
[SIZE=4]AllocationBase 0x0, BaseAddress 0x71110000, RegionSize 0x480000, State 0x10000[/SIZE]
[SIZE=4]C:\nxp\LPCXpresso_4.0.5_123\lpcxpresso\msys\bin\make.exe: *** Couldn't reserve space for cygwin's heap, Win32 error 487[/SIZE][/LEFT]

[LEFT][SIZE=4]**** Build of configuration Debug for project adc ****[/SIZE][/LEFT]

[LEFT][SIZE=4]I do have Cygwin installed and just updated. This has not been a problem in the past.[/SIZE]
[SIZE=4]I also have previous versions of LPCXpresso installed in seperate directories.[/SIZE][/LEFT]
[SIZE=4]I have lots of free disk space and RAM.[/SIZE]

[LEFT][SIZE=4]Any thoughts?[/SIZE]
[SIZE=4]Pete.[/SIZE][/LEFT]
0 项奖励
回复
2 回复数

780 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by micrio on Wed Jun 29 10:57:47 MST 2011
That did fix it!

Thanks,
Pete.
0 项奖励
回复

780 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Jun 29 10:43:13 MST 2011
Solution:

http://support.code-red-tech.com/CodeRedWiki/VirtualAllocPointerNull
0 项奖励
回复