Pin read

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Pin read

1,884件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ivangeorgiev on Fri Apr 17 13:42:55 MST 2015
How can I check the value of the pin j6-29?
0 件の賞賛
返信
6 返答(返信)

1,867件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ivangeorgiev on Fri Apr 17 15:02:24 MST 2015
I see... Maybe the button is connected to another pin or they gave me something that's not connected properly. Thank you for the help  :)
0 件の賞賛
返信

1,867件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Fri Apr 17 14:52:18 MST 2015

Quote: ivangeorgiev
There is a button connected to what I think is pin j6-29.



Schematic of LPCXpresso1769 board is describing that J6-29 is not used  :)

0 件の賞賛
返信

1,867件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ivangeorgiev on Fri Apr 17 14:44:37 MST 2015
I am using a LPC1769 LPCXpresso board. There is a button connected to what I think is pin j6-29. I want to read when the button has been pressed. Here is a image of what I have http://postimg.org/image/ldnher5lz/
0 件の賞賛
返信

1,867件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Fri Apr 17 14:32:47 MST 2015

Quote: ivangeorgiev
I want to make a program using LPCExpresso. I know how to check the value if the pin is part of a port, but j6-29 is not. What commands should I use?



:quest:

Could be useful to give us a hint which hardware you are using...
0 件の賞賛
返信

1,867件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ivangeorgiev on Fri Apr 17 14:23:41 MST 2015
I want to make a program using LPCExpresso. I know how to check the value if the pin is part of a port, but j6-29 is not. What commands should I use?
0 件の賞賛
返信

1,867件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Fri Apr 17 13:51:12 MST 2015

Quote: ivangeorgiev
How can I check the value of the pin j6-29?



:quest:

Write a program or use the debugger....
0 件の賞賛
返信