PWM on LPC1751

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PWM on LPC1751

910件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tinto on Wed Mar 21 03:44:50 MST 2012
Hai...

Is there any way to generate 6 PWMs with different frequencies using LPC1751?
I don't need to change the duty cycle. I just need to have independent frequencies in each channel.
0 件の賞賛
返信
3 返答(返信)

901件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gbm on Wed Mar 21 07:02:01 MST 2012
AFAIR, you may generate one PWM frequency in hardware using PWM and 3 using MCPWM. If two more are needed, you can do it in software using two other timers. No problem if you don't require extremely small jitter.
0 件の賞賛
返信

901件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tinto on Wed Mar 21 05:10:45 MST 2012
Ok, I agree with that.

But any simple method to generate 6 PWMs with different frequencies in software?
I need frequency below 5kHz only.
0 件の賞賛
返信

901件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Mar 21 04:08:29 MST 2012
No :eek:

Answered already in: [U]http://knowledgebase.nxp.com/showthread.php?t=2392[/U]
0 件の賞賛
返信