Now Available: LPCXpresso for MAC OS X

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Now Available: LPCXpresso for MAC OS X

1,081件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by derrick.oliver on Thu Jul 12 15:27:24 MST 2012
[B][B]NXP is proud to announce LPCXpresso for MAC OS X. [/B][/B]

In response to the high volume of user requests, NXP and Code Red are  proud to announce the immediate availability of LPCXpresso for Mac OS  X. Combined with the existing Windows and Linux support, this makes  LPCXpresso a true multi-platform development environment.

To download and for more information, visit: [U]http://www.lpcware.com/content/project/nxp-lpcxpresso[/U]
0 件の賞賛
返信
1 返信

759件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by trigger on Sat Feb 02 05:46:56 MST 2013

Quote: derrick.oliver
[B][B]NXP is proud to announce LPCXpresso for MAC OS X. [/B][/B]

In response to the high volume of user requests, NXP and Code Red are  proud to announce the immediate availability of LPCXpresso for Mac OS  X.




I'm running LPCXpresso IDE 5 on OS X, thank you for supporting that platform. But, I now realized I do not have an upgrade option to the "NXP Edition" of Code Red, as they are only supported on Windows. The "Full" version runs on OS X, but not the "NXP Edition".

Is there any reason for this restriction? Would be nice to have an upgrade path from LPCXpresso IDE to the Code Red NXP Edition on a Mac.

Thanks
Andrej
0 件の賞賛
返信