No emulator/board available

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No emulator/board available

1,041 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by reLinux on Fri May 18 12:29:22 MST 2012
Hello all,

I installed LPCXpresso successfully on my Ubuntu 10.04 some time ago and was able to debug programs on my LPC11C24. Now, after several weeks and Ubuntu-Updates that does no longer work. I always get the "No emulator/board available" message.

I tried different USB ports and cables. I also tried to pull P0_1 low to get into ISP mode without success.

Following http://support.code-red-tech.com/CodeRedWiki/LPCLinkDiagnostics gives the following results:

$ lsusb
Bus 001 Device 050: ID 0471:df55 Philips
$ ./dfu-util -l
dfu-util - (C) 2007-2008 by OpenMoko Inc.
This program is Free Software and has ABSOLUTELY NO WARRANTY

Found Runtime: [0x0471:0xdf55] devnum=50, cfg=0, intf=0, alt=0, name="UNDEFINED"

$ ./dfu-util -d 0x471:0xdf55 -c 0 -t 2048 -R -D LPCXpressoWIN.enc
dfu-util - (C) 2007-2008 by OpenMoko Inc.
This program is Free Software and has ABSOLUTELY NO WARRANTY

Opening USB Device 0x0471:0xdf55...
Claiming USB DFU Runtime Interface...
Determining device status: state = dfuIDLE, status = 0
WARNING: Runtime device already in DFU state ?!?
Found Runtime: [0x0471:0xdf55] devnum=50, cfg=0, intf=0, alt=0, name="UNDEFINED"
Claiming USB DFU Interface...
Setting Alternate Setting ...
Determining device status: state = dfuIDLE, status = 0
dfuIDLE, continuing
Transfer Size = 0x0800
bytes_per_hash=604
Starting download: [##################################################] finished!
state(8) = dfuMANIFEST-WAIT-RESET, status(0) = No error condition is present
Done!
can't detach: error sending control message: Broken pipe
Resetting USB to switch back to runtime mode

$ lsusb
Bus 001 Device 051: ID 1fc9:0009
$ export CRT_DEBUG_TRACE=1
$ ./crt_emu_lpc11_13_nxp -info-emu -wire=winusb
Ni: LPCXpresso Debug Driver v4.0 (Mar 25 2012 14:25:38)
0 Emulators available:

I think, that dfu-util fails booting the debugger firmware, but why and what can I do to get it running again?

Kind regards

Stephan
0 Kudos
Reply
3 Replies

1,005 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dragilla on Thu Jul 26 03:38:55 MST 2012
I have the same problem now. It works 1-2 days after install. Then it fails with the error message: "No emulator/board available.
This could be because it is unpowered, disconnected or already in use".
Reinstall helps and it works again for 1-2 days.

I think it's something with ubuntu (12.04 here) and permissions...
0 Kudos
Reply

1,005 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by reLinux on Sun Jun 03 09:08:45 MST 2012
Hallo all,

it turned out that there was something broken in the installation. After a new installation with the same Ubuntu on my laptop worked I tried to reinstall the software on the desktop computer and the problem was gone.

Kind regards

Stephan
0 Kudos
Reply

1,005 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by whitecoe on Sat May 19 00:00:16 MST 2012
Its a bit long, but it might be worth working your way through this recent thread....

http://knowledgebase.nxp.com/showthread.php?t=3132

HTH!
0 Kudos
Reply