No Output while debugging semihosting project (5.0.10_1022)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No Output while debugging semihosting project (5.0.10_1022)

2,198 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mrib on Thu Nov 22 13:16:39 MST 2012
Hi all!

On Ubuntu 12.04 (64Bit) I installed LPCXpresso 4.3.0_1025 and the hello world semihosting project displays the output of printf on console in the IDE (as expected).

After installing LPCXpresso 5.0.10_1022 (new workspace and new semihosting hello world project generated by the wizard) there is no output on the console.

Do I missed something or can anybody confirm this behavior?

Thanx, mrib
0 Kudos
Reply
10 Replies

2,182 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mrib on Fri Nov 23 13:44:12 MST 2012

Quote: CodeRedSupport
Sorry about that - now fixed.


Thanks a lot! Semihosting is working now (Ubuntu 12.04 64bit, LPCXpresso lpc1768).
0 Kudos
Reply

2,182 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Fri Nov 23 12:37:32 MST 2012
Sorry about that - now fixed.
0 Kudos
Reply

2,182 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mrib on Fri Nov 23 11:38:37 MST 2012

Quote: CodeRedSupport
5.0.12, which fixes this issue, is now available.


Thanks very much for the quick bug fixes. These are great news for the weekend! I'll try immediately the semihosting issue.

Unfortunately the link to the new Linux package seems to be broken...
0 Kudos
Reply

2,182 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Fri Nov 23 10:18:31 MST 2012
5.0.12, which fixes this issue, is now available.
0 Kudos
Reply

2,182 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Fri Nov 23 02:16:36 MST 2012

Quote: mrib
Hi all!

On Ubuntu 12.04 (64Bit) I installed LPCXpresso 4.3.0_1025 and the hello world semihosting project displays the output of printf on console in the IDE (as expected).

After installing LPCXpresso 5.0.10_1022 (new workspace and new semihosting hello world project generated by the wizard) there is no output on the console.

Do I missed something or can anybody confirm this behavior?

Thanx, mrib



I can confirm that this was a bug in 5.0.10 on Linux. It has been fixed and a new version will be available very soon.

Apologies for the inconvenience.
0 Kudos
Reply

2,182 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fjrg76 on Thu Nov 22 16:56:49 MST 2012
http://support.code-red-tech.com/CodeRedWiki/UsingPrintf
0 Kudos
Reply

2,182 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mrib on Thu Nov 22 14:43:11 MST 2012

Quote: kayoda
Did you try to import the working project in V5.0?


The import of the working project from V4 into V5 workspace has the same effect: no output to console...
0 Kudos
Reply

2,182 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mrib on Thu Nov 22 14:40:24 MST 2012

Quote: fjrg76
Quick Settings-> Set library type -> Redlib semihost


I checked Redlib semihost in the linker part of project config. --> no success
0 Kudos
Reply

2,182 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ex-kayoda on Thu Nov 22 14:17:10 MST 2012
Did you try to import the working project in V5.0?
0 Kudos
Reply

2,182 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fjrg76 on Thu Nov 22 14:12:36 MST 2012
Quick Settings-> Set library type -> Redlib semihost
0 Kudos
Reply