Newbie quesitons for LPCXpresso IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Newbie quesitons for LPCXpresso IDE

1,599件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rocketman46 on Thu Apr 10 00:10:12 MST 2014
Hi All,

I am just moving over to ARM and LPCXpresso from a another manufacturer/ technology and I need to ask a few questions, some very newbie questions.

1) Does the free LPCXpresso cover all the NXP ARM range.  I am mainly interested interested in the Cortex M0 and M3, but would like to know what chips are covered or not.

2) Does the LPCXpresso IDE connect to any debugger, or only the NXP debugger?

3) Does the free LPCXpresso version have the same libaries as the full version but is on code limited to 256KB.

Thanks in advance.

Regards,

rocketman46
0 件の賞賛
返信
8 返答(返信)

1,587件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Apr 11 09:02:49 MST 2014
You need nothing other than a USB cable. The Debug Probe is built into ALL mbed boards and is known as CMSIS-DAP.
0 件の賞賛
返信

1,587件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rocketman46 on Fri Apr 11 08:55:20 MST 2014
Hi,

Thanks for your reply.

So do you mean I don't need a debugger it will work with the usb cable only.

Or yes any of the above debuggers will work with no additional modifications?

Thanks for your input.

0 件の賞賛
返信

1,587件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Apr 11 07:56:05 MST 2014
You don't need anything else. You can connect directly to the USB port and the debugger will recognise and will be able to debug your target.
0 件の賞賛
返信

1,587件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rocketman46 on Fri Apr 11 07:33:08 MST 2014
Hi, sorry for the lack of details.  The board is below:

I am new to ARM and lpcxpresso so still learning.  So if I use lpcxpresso, and the board below, what debugger/ programmer would you recommend?  I see there is J-link, J-link 2 and code red + but not sure on whats good?  I am hobby level so not really after an expensive debugger/ programmer.  Over £100 pounds is pushing it.

Anyway if you could give your feedback on the pros and cons and how I would connect this debugger up to this board and lpcxpresso.  I am not sure if it is plug and play or changes are required.

https://mbed.org/platforms/mbed-LPC1768/

Regards,
0 件の賞賛
返信

1,587件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Apr 11 05:37:35 MST 2014
The mbed boards support CMSIS-DAP, so yes, you can connect a debugger to the mbed board.
0 件の賞賛
返信

1,587件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Fri Apr 11 05:29:42 MST 2014

Quote: rocketman46
... a dev board with a NXP M3 chip...


Will the above mentioned debuggers in 2 fit on this board, or would I need to make an additional connection?



:quest:

If you give us a hint which magic board you've bought, the answer is easy...
0 件の賞賛
返信

1,587件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rocketman46 on Fri Apr 11 05:23:02 MST 2014
Ok thanks for your reply.

I have just bought a dev board with a NXP M3 chip on it.  The board is supposed to be programmed via USB using mbed but I prefer my code secure on my PC and not on the cloud.

Will the above mentioned debuggers in 2 fit on this board, or would I need to make an additional connection?

Regards,
0 件の賞賛
返信

1,587件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Apr 10 00:58:00 MST 2014
1. Yes
2. LPC-Link, LPC-Link2, Red Probe+ and CMSIS-DAP. Just announced is the ability to connect to Segger J-Link
3. Yes
0 件の賞賛
返信