Need a lpc1769 target

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need a lpc1769 target

1,040 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by hellospencer on Fri Aug 17 06:05:11 MST 2012
Hello,

Are there 'lpcexpresso target side boards only' up for sale? I do not want to build (and solder!) my own PCB, but rather connect existing pieces.

If not, are there freely available and correct design files for the lpc 1769?

Cheers

UPDATE:

The mbed project provides hardware as well as schematics for such purposes.
0 Kudos
Reply
2 Replies

1,025 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Polux rsv on Mon Aug 20 00:18:25 MST 2012
Given the board's price, buy a complete LPCXpresso board and cut it to use only the target side.

Angelo
0 Kudos
Reply

1,025 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ex-kayoda on Fri Aug 17 06:14:23 MST 2012

Quote: hellospencer
Are there 'lpcexpresso target side boards only' up for sale?



No :mad:


Quote: hellospencer

If not, are there freely available and correct design files for the lpc 1769?



No :( (Only schematic :))
0 Kudos
Reply