Need Help for the issue: Can't get response from controller after uploading project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need Help for the issue: Can't get response from controller after uploading project

819 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Irene_Envio on Fri Dec 04 18:17:42 MST 2015
Hello,

Could I have someone helping me with this issue? :) Thank you in advance!

I have LPC_Linek 2, controller (PCB), LPCXPRESSO and CoolTerm which shows the feedback of a command directly. Previously, I could upload my code to my PCB, and get responds from the controller when commands were sent.   After I uploaded modified version of the code that only had a few simple commands added on, I can still upload the code, but I can't get any response from my controller anymore, even I tried to upload the old version of my code, and it doesn't work either.

Could someone give some suggestions to solve this issue?

Thank you!
I really need to solve it as soon as possible.


0 Kudos
Reply
2 Replies

810 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Fri Dec 04 20:47:22 MST 2015
Please detail HOW the problem was solved so as to help other people who might have the same problem.

Regards, Mike.
0 Kudos
Reply

810 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Irene_Envio on Fri Dec 04 19:50:15 MST 2015
Problem sloved!
Thanks
0 Kudos
Reply