Mistake in sample code for Motor control pwm

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mistake in sample code for Motor control pwm

684件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fduignan on Wed Dec 07 08:35:21 MST 2011
The sample motor control pwm code supplied with LPCXpresso has a mistake.  The correction is shown below (file: mcpwm.c, Project: NXP LPC17xx Motor Control PWM example )
Corrected code:

void MCPWM_Init(void)
{
  LPC_SC->PCONP |= 0x00020000;           /* Turn On MCPWM PCLK */

  /* P1.19~1.26, P1.28~29 as Motor Control PWM pins. */
  LPC_PINCON->PINSEL3 &= ~(0xFFFF<<6);
  // LPC_PINCON->PINSEL3 &= ~(0x5555<<6); // Does not make any sense
  LPC_PINCON->PINSEL3 |= (0x5555<<6);      // This is the correct way

  LPC_PINCON->PINSEL3 &= ~(0x0F<<24);
  // LPC_PINCON->PINSEL3 &= ~(0x05<<24); // Does not make any sense
  LPC_PINCON->PINSEL3 |= (0x05<<24);     // This is the correct way
  return;
}
0 件の賞賛
返信
0 返答(返信)