Missing SPI1 in Peripherals+ tab

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Missing SPI1 in Peripherals+ tab

628 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rogerwilson on Sat Sep 26 14:06:49 MST 2015
I have an LPC1113/302 project using SPI1. The SPI1 peripheral is still missing from the Peripherals+ tab.

Missing SPI1 has been reported before. When is this going to be solved please?

Rog.
0 Kudos
Reply
2 Replies

622 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rogerwilson on Tue Sep 29 01:17:55 MST 2015
Thanks for the reply and advice on how to get around the problem.

I was thinking of this thread when I said it had been mentioned before:
https://www.lpcware.com/content/forum/missing-spi1-peripherals-view-lpc1114301

Thanks,

Rog.
0 Kudos
Reply

622 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Sep 28 01:45:14 MST 2015
Indeed, it looks like SPI1 is not there in the LPC1113/302 Peripherals view in LPCXpresso 7.9.2 and earlier.

I can't find any report of missing SPI1 on the LPC1113/302 part previously. But I can see why this may have been missed when the definitions were original created - as SPI1 is only accessible on the 48 pin package.

Anyway, we'll look into getting it added to the the Peripherals view for the LPC1113/302 in the next LPCXpresso release.  In the short term, you may be able to just set your MCU to something like LPC1113/303 (which has the same flash/ram size). From a tools viewpoint, this should be the same.

Regards,
LPCXpresso Support

0 Kudos
Reply