Missing Coil

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Missing Coil

584件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bobi-one on Thu Jun 10 00:31:17 MST 2010
I purchased Lpcxpresso with lpc1343 and I noticed that there are no Coils (L1 L2) soldered. Are they crucial for the operation of the LPClink ?
0 件の賞賛
返信
1 返信

578件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Jun 10 00:59:11 MST 2010

Quote: bobi-one
I purchased Lpcxpresso with lpc1343 and I noticed that there are no Coils (L1 L2) soldered. Are they crucial for the operation of the LPClink ?



No. These were fitted on the original batches of LPCXpresso boards, but have since been removed. For more details see:

http://knowledgebase.nxp.com/showthread.php?t=166

Regards,
CodeRedSupport
0 件の賞賛
返信