Maximum current from VIO_3V3X

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Maximum current from VIO_3V3X

934 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lsimons on Wed Feb 01 11:58:56 MST 2012
I am prototyping a design with an LPCXpresso 1769 board, and was wondering how much current can be provided by the VIO_3V3X (VOUT) pin on the board?  I have found schematics for the target side of the board, but can't seem to find details on the emulation side and what kind of power supply it provides.

Thanks,
Louis
0 Kudos
Reply
4 Replies

923 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lsimons on Wed Feb 01 13:55:38 MST 2012

Quote: Zero
That's no problem. IIRC I've connect >150mA already. It's just important to reduce power while flashing (with low active Chip Select... ) :rolleyes:



That's good news, thanks!
0 Kudos
Reply

923 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Feb 01 13:08:41 MST 2012

Quote: lsimons
...50 mA...



That's no problem. IIRC I've connected >150mA already. It's just important to reduce power while flashing (with low active Chip Select... ) :rolleyes:
0 Kudos
Reply

923 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lsimons on Wed Feb 01 13:01:01 MST 2012
Thanks for the link.  I'm looking for around 50 mA to drive a fairly high power LED (worst case scenario).

So, given the CAT6219's (http://www.onsemi.com/pub_link/Collateral/CAT6219-D.PDF) 500mA tops, at 5V from the computer and 3.3V out, there's 0.85W trying to get out.  The thermal resistance says there should be a temperature rise of 200C, which is well above the junction temperature range, which should put the chip in thermal shutdown.  Maybe there's some diodes in the path dropping voltage (dissipating power) along the way.

Anyway, looks like I have enough to make the power budget work without being too close to the edge.
0 Kudos
Reply

923 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Feb 01 12:47:00 MST 2012
How much current do you need?

See #6 of http://knowledgebase.nxp.com/showthread.php?t=2614
0 Kudos
Reply