Max. speed CAN_clk

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Max. speed CAN_clk

902件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by luky on Thu Sep 01 23:56:35 MST 2011
I have a LPCXpresso with the LPC11C24, but I have changed the Oscillator to 20MHz to run the Chip at 50MHz. Now I want to use the C_CAN Module (Baudrate 50k) and I have Problems to select the correct Register values.
What is the max. frequency (or recommended frequency) for the CAN-Module? All examples use 8MHz, but that won't work in my case.
Is there a chance to get 50k Baudrate with minmimal Tolerances with the 20MHz Crystal Oscillator or should I change it back to 12MHz?
0 件の賞賛
返信
0 返答(返信)