MCU without crystal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCU without crystal

990件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Thu Jan 12 09:39:10 MST 2012
Hello all,

I can leave the crystal input (XI) disconnected when not in use? The processor (LPC111x) takes care automatically?

Thank you.
0 件の賞賛
返信
3 返答(返信)

980件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Thu Jan 12 20:59:05 MST 2012
Yes, that was the experiment: put a bridge between the capacitor pads of the crystal pin XI.
0 件の賞賛
返信

980件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gbm on Thu Jan 12 12:57:36 MST 2012
A better idea is to connect XIN to ground, to set input of CMOS amplifier to some reasonable state.
0 件の賞賛
返信

980件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Thu Jan 12 12:46:26 MST 2012
I did some experiments:
- Necessary to use the XI pin.
- Energy consumption decreased 1 mA.

Very well, thank you for your attention. :)
0 件の賞賛
返信