M0 flash driver can not be set in multi core app

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

M0 flash driver can not be set in multi core app

494 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by askar on Thu May 29 23:59:19 MST 2014
Hi,

for creating multi core application for lpc4357,
in Free edition of lpcxpresso version 7.0.0, first i created a project for m0
then i created project for m4 and set the loading address for m0 to be flash2.
i compiled m0 without any error, then compiled m4 and there was
"M0APP execute address differs from address provided in source image" i checked mcu setting in m0 and saw that
flash driver is set to bank A, i tried many times to set flash driver to bank B but with no success.
any help is appreciated in advance.

best regards,
0 Kudos
Reply
1 Reply

441 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri May 30 01:06:20 MST 2014
Please read the FAQ:
http://www.lpcware.com/content/faq/lpcxpresso/lpc43xx-multicore-apps

Also, I suggest you compare the configuration of your project with the LPC4357 multicore example, shipped in the product (Keil_MCB4357.zip).
0 Kudos
Reply