LpcXpresso and plugins

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LpcXpresso and plugins

1,532件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by micronpn on Sat Feb 08 05:05:48 MST 2014
I have problems to install plugins on LpcXpresso LPCXpresso v6.1.4 [Build 194] [2014-01-15].
There are a lot of useful plugins for Eclipse that I normally use in Eclipse and in previous LpcXpresso releases.

The more important for me are Atlassian (a plugin to connect to JIRA and Confluence servers), Mylyn, Egit, Eclox and Natural (it requires Xtext also).

This is the error I have installing Atlassian plugins:

Cannot complete the install because one or more required items could not be found.
  Software currently installed: LPCXpresso 6.1.4.201401140032 (com.crt.lpcxpresso.juno.cross 6.1.4.201401140032)
  Missing requirement: LPCXpresso 6.1.4.201401140032 (com.crt.lpcxpresso.juno.cross 6.1.4.201401140032) requires 'com.crt.lpcxpresso.juno.cross.root.feature.feature.group [6.1.4.201401140032]' but it could not be found

This for Egit and/or Mylyn:

Cannot complete the install because one or more required items could not be found.
  Software currently installed: LPCXpresso 6.1.4.201401140032 (com.crt.lpcxpresso.juno.cross 6.1.4.201401140032)
  Missing requirement: LPCXpresso 6.1.4.201401140032 (com.crt.lpcxpresso.juno.cross 6.1.4.201401140032) requires 'com.crt.documentation.feature.group [6.1.4.201401140032]' but it could not be found

and so on.

I assumed that every update should be downloaded from Juno update site.

1. Why in the newer releases there are so many problems to install a plugin?
2. Where can I find and where can I add the missing modules?
0 件の賞賛
返信
4 返答(返信)

1,363件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by micronpn on Tue Feb 11 04:17:50 MST 2014
I didn't know this Windows rule, I supposed that every application with a JVM in its path should use it instead of the JVM installed in the PC. Now I can understand some mistakes I have also in other applications. Unfortunately there are too much applications requiring JVM running so this should mean that the 1st JVM started will be used. Good to know.
Should be good to stop the JVM already running, I searched around the web but seems that to stop it I should be able to stop the application that launched the JVM. Do you know a way to stop it anyway?
0 件の賞賛
返信

1,363件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Feb 10 11:29:21 MST 2014
If an instance of a JVM is already running, Eclipse (LPCXpresso) will use it (AFAIK, this is a Windows/Java restriction of not being able to have multiple JVMs running at the same time). If there is no JVM running, Eclipse will use the one found in the 'jre' subdirectory.

So, you should either
- sort out the problems in you existing JVM installation, or
- start LPCXpresso first, so it uses the one supplied
0 件の賞賛
返信

1,363件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by micronpn on Mon Feb 10 10:37:55 MST 2014
I found that errors I had were related to missing Java files. Very strange because LpcXpresso has its own Java installed and it was a fresh installation. The problems may be solved copying the missing files or repeating the installation.
0 件の賞賛
返信

1,363件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Feb 10 01:55:28 MST 2014
I just installed the Atlassian plugin from:
http://update.atlassian.com/atlassian-eclipse-plugin/rest/e3.7
the Egit plugin from:
http://download.eclipse.org/egit/updates
and the Mylyn support from:
http://download.eclipse.org/mylyn/releases/lates

(in that order) into a clean install of LPCXpresso 6.1.4 on Windows without any problems.

Can you please install a clean version of LPCXpresso 6.1.4 and try again. If you have problems, can you please explain EXACTLY what you did to produce the problem?
0 件の賞賛
返信