Lpc1769 Link USB device driver for win xp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Lpc1769 Link USB device driver for win xp

2,517件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Henry on Sun Dec 11 20:19:41 MST 2011
Hi All,
I bought LPC1769 link with LPCXpresso base board.
I have HP deck top computer with window xp media center version.
When I connect LPC1769 link with that computer.
USB device driver installation is appeared and installation is failed again and again.
Where can I have this USB device driver for window xp?
Please help me.
0 件の賞賛
返信
4 返答(返信)

2,231件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Henry on Wed Dec 14 22:57:39 MST 2011
Dear Sir,

I got it. It works after I follow as per your instruction.
I also realise that LPC link v1.1 also need to be installed.
Anyway, thanks a lot. My one of 2 windows Xp computers is working properly.
Thank you.

Henry
0 件の賞賛
返信

2,231件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Dec 13 05:45:42 MST 2011
It looks like the driver has not been installed. This could be because
- you did not let the driver install when you installed LPCXpresso. Try re-installing the drivers (hint: use Device Manager to show the devices and you can update/install the driver from there. The drivers are in the LPCXpresso directory)
- the driver installation failed because of Windows driver database corruption. If the above fails to correct the problem, then your driver database is likely to be corrupt. This requires a re-install of Windows to correct (and is nothing to do with LPCXpresso)
0 件の賞賛
返信

2,231件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Henry on Tue Dec 13 05:29:09 MST 2011
Dear Sir,

I found below message in windir setup.api.log.

[2011/12/12 10:22:07 464.441]
#-198 Command line processed: "C:\WINDOWS\system32\mmc.exe" C:\WINDOWS\system32\devmgmt.msc /s
#I060 Set selected driver.
#-019 Searching for hardware ID(s): usb\vid_0471&pid_df55&rev_0001,usb\vid_0471&pid_df55
#-018 Searching for compatible ID(s): usb\class_fe&subclass_01&prot_00,usb\class_fe&subclass_01,usb\class_fe
#-166 Device install function: DIF_SELECTBESTCOMPATDRV.
#W059 Selecting best compatible driver failed. Error 0xe0000228: There are no compatible drivers for this device.
#W157 Default installer failed. Error 0xe0000228: There are no compatible drivers for this device.
#-166 Device install function: DIF_SELECTBESTCOMPATDRV.
#W059 Selecting best compatible driver failed. Error 0xe0000228: There are no compatible drivers for this device.
#W157 Default installer failed. Error 0xe0000228: There are no compatible drivers for this device.
#I060 Set selected driver.
#-019 Searching for hardware ID(s): usb\vid_0471&pid_df55&rev_0001,usb\vid_0471&pid_df55
#-018 Searching for compatible ID(s): usb\class_fe&subclass_01&prot_00,usb\class_fe&subclass_01,usb\class_fe
#-166 Device install function: DIF_SELECTBESTCOMPATDRV.
#W059 Selecting best compatible driver failed. Error 0xe0000228: There are no compatible drivers for this device.
#W157 Default installer failed. Error 0xe0000228: There are no compatible drivers for this device.
#-166 Device install function: DIF_SELECTBESTCOMPATDRV.
#W059 Selecting best compatible driver failed. Error 0xe0000228: There are no compatible drivers for this device.
#W157 Default installer failed. Error 0xe0000228: There are no compatible drivers for this device.

May I know what it means? You said ten of thousand of computers are OK. But why my one like that happens? What can I do more? Please help me.
Thank you.
0 件の賞賛
返信

2,231件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon Dec 12 01:00:11 MST 2011
There are no known problems with the LPC-Link drivers - they have been installed on tens of thousands of machines without any problems. Therefore, the most likely reason for your driver install failing is that Windows XP driver database on your PC is corrupted. If it is, AFAIK the only solution is a clean install of Windows.

To confirm this, you can look in %windir%\setupapi.log which is the installation log for all device drivers on XP and look for the error messages.
0 件の賞賛
返信