Lpc11c14 - header files

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Lpc11c14 - header files

1,117件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kenako on Mon Jun 28 07:21:11 MST 2010
For the LPC11C14, do you know if LPCXpresso supports the device yet? I know it supports the
LPC11xx range, however I checked the library files in the software and the LPC11C14 Header files are not implemented  yet ? The only
additions would be the pointers associated with the CAM block.
0 件の賞賛
返信
1 返信

1,082件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jdebliek on Mon Jun 28 12:44:14 MST 2010
I am just finishing a project with the LPC11C14.  The NXP rep had sent me the sample code the Keil and IAR generated for the part.  Attached is the header file I used.  I think I had to add the interrupt definitions to the initial file I received.

The Keil code I received does not use the CAN ROM functions, but the IAR code does.  If you plan on using the ROM functions, I would recommend getting the IAR code, as the user manual is somewhat deficient.  I did not receive this code until after a spend several days figuring it out myself.
0 件の賞賛
返信