Lpc 1343 usb hid & isp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Lpc 1343 usb hid & isp

758 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by alanbithell on Fri Aug 19 05:01:01 MST 2011
I have a working system with USB HID, i use the HID to configure my board and program some external flash memory via spi. I want to invoke ISP via a HID command. Calling the function from a HID command is easy, but i dont get the device enumerating as a MSC, my HID just stays there, even though it has entered the ISP as my heartbeat led stops and i loose connection to the debugger. Why isnt it entering ISP correctly? any ideas?
0 Kudos
Reply
1 Reply

726 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Fri Aug 19 14:35:24 MST 2011
Hi,

Please refer to the app note/software example below.
See if this works.

http://ics.nxp.com/support/documents/microcontrollers/zip/an10986.zip

This app note shows how to use the USB ISP feature.
Thanks.
0 Kudos
Reply