Linux software to talk to the boot loader ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linux software to talk to the boot loader ?

945 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ataru on Thu Dec 02 17:23:40 MST 2010
LPC11C14 connected to a Linux host system through the serial port. Application: CAN to serial bridge.

For ease of production and field updates, we would like to program the device in-circuit, using the serial port and the built-in boot loader.

The controller should always go into boot loader first, then the application running on the Linux host can decide whether it needs to update the firmware, or start the flash code on the LPC11C14.

Is there any canned Linux code for this that we can adapt ? I would rather not reinvent this wheel...
0 Kudos
Reply
2 Replies

922 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by domen on Tue Dec 07 03:20:13 MST 2010

Quote: igorsk
I hear that lpc21isp can be compiled for Linux.



Jup, lpc21isp works quite fine. Tested with lpc1343 and lpc1114 here.
0 Kudos
Reply

922 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by igorsk on Mon Dec 06 05:11:37 MST 2010
I hear that lpc21isp can be compiled for Linux.
0 Kudos
Reply