LPCxpresso LPC1769 and TCP/IP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCxpresso LPC1769 and TCP/IP

1,279件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by markustmaier on Tue Sep 11 09:25:16 MST 2012
Hello,

I'm looking for an easy implementation of a TCP/IP stack for the LPCxpresso LPC1769 and Baseboard from Embedded Artists. I aim to use simple TCP send and receive commands to communicate with a motor controller.

I have to communicate with three of these motor controllers, so I should be able to open three different connections. The commands are realy simple like "HORM".

Which stack is the best for this application? Speed is not a issue. Which stack can be understand easier?
- lwIP
- uIP
- EasyWeb

Is there anybody who has source code for one of these stacks? I'm new to ethernet and I like to have two little functions: TCP_Send and TCP_Receive where I can send and receive strings via TCP. There is enough to do with the coding of the other parts, so the ethernet part should be as easy as possible.

Thanks!

Markus
0 件の賞賛
返信
3 返答(返信)

1,011件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Fri Nov 02 03:52:05 MST 2012

Quote: markustmaier
Is there a easy way to do this?



AFAIK No :o

EasyWeb is including http and therefore TCP. To send / receive data it's useful to understand what TCP is and how it works. So it can be useful to read TCP parts of EasyWeb. If you are looking for a simple way, try mbed :)
0 件の賞賛
返信

1,011件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by markustmaier on Fri Nov 02 03:29:57 MST 2012
Hi,

thanks for the link. I've already looked at the app note. But I don't understand how I can send and receive TCP strings.

Is there a easy way to do this? Maybe an idea where I can look at those funtions?

Thanks!
0 件の賞賛
返信

1,011件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by daniel.widyanto on Fri Sep 28 01:04:26 MST 2012
Hi Markus,

See this app note: http://www.nxp.com/documents/other/uip_webserver_src_lpc1700.zip
0 件の賞賛
返信