LPCXpresso v4.05 CMSISv2 install

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso v4.05 CMSISv2 install

1,091件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rattus on Mon Jul 25 12:51:39 MST 2011
Hi - I just installed LPCXpressov 4.05, and when I try the New Project wizard, it fails with "Dependent project CMSISv2p00_LPC17xx not found..."

I have unzipped the CMSISv2 library as a subdirectory under my project workspace. What am I doing wrong?

Thanks,

Mike
0 件の賞賛
返信
4 返答(返信)

1,077件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Fri Apr 06 03:21:08 MST 2012
This is described in the Getting Started that is provided with the project. It is even available from the Welcome page that is opened every time you start the IDE.

In the Quickstart panel, press the Import button
Browse to NXP/LPC1000/LPC17xx (or whatever target you want) and you will find a bunch of examples there.

These all work out of the box.
0 件の賞賛
返信

1,077件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lipny on Fri Apr 06 02:26:04 MST 2012

Quote: Zero
The magic word is 'IMPORT'. Just import CMSIS as described in GettingStarted :)



1. IMPORT what ? and what page of which version of the G.S. ? I tried to import the hole bunch of stuff and still the same errror.

Why don;t you have an example PROJECT that can be OPENED and everything will just WORK at first launch. This is pathetic ...
0 件の賞賛
返信

1,077件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rattus on Mon Jul 25 13:11:32 MST 2011
...answered that one myself - I needed to import the CMSISv2p00_LPC17xx directory as a project *before* starting a new project.

<edit> Thanks Zero, seems we were typing at the same time. Read a manual, are you nuts? ;-)

Mike
0 件の賞賛
返信

1,077件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Mon Jul 25 13:04:55 MST 2011

Quote: rattus
...I have unzipped the CMSISv2 library...

What am I doing wrong?




The magic word is 'IMPORT'. Just import CMSIS as described in GettingStarted :)
0 件の賞賛
返信