LPCXpresso v3.6.0 released

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCXpresso v3.6.0 released

765 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Dec 14 07:42:25 MST 2010
LPCXpresso v3.6.0 for Windows has been released. Changes in the release include:

[LIST]
[*]Improved support for LPC177x/8x
[*]Major revamp of linker script generation to support multiple memory  regions, CRP and reserved memory regions for ROM-based drivers.See Enhanced Managed Link Scripts FAQ for more information
[*]Update to startup files to match new linker scripts
[LIST]
[*]NOTE: existing startup files will continue to work with new linker scripts.
[/LIST]

[*]Fix for occasional display of empty Core Register view when debugging
[*]Fix issue with displaying peripherals containing write-only or volatile registers
[/LIST]
The equivalent Linux release will follow in a few days.
0 项奖励
回复
1 回复

755 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Dec 16 03:24:14 MST 2010
LPCXpresso for Linux (Version 3.8.0 build 114) is now available for download from http://lpcxpresso.code-red-tech.com/LPCXpresso/

This contains the new features described previously in this thread for LPCXpresso v3.6.0 on Windows.
0 项奖励
回复