LPCXpresso v3.4.0 released

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso v3.4.0 released

1,149件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Jun 24 00:50:43 MST 2010
We are pleased to announce the release of LPCXpresso v 3.4.0.

Major changes in this release include:

[LIST]
[*]Added support for LPC2929 and LPC3250
[*]Added new 'reset after programming' option to Flash dialog
[*]Fix to Managed linker script for data section
[*]Various fixes/improvements to peripheral descriptions
[*]Debugger fixes for problems related to stepping and viewing  variables
[*]Fixed problem with setjmp in C library
[*]Fixed a rare activation issue. Note: Customers who experienced this  problem with previous releases may need acquire a new serial number and  activation key.
[*]Note: If you are upgrading from a previous installation, we  recommend that you install into a new directory. You will be able to use  any existing workspaces, and your existing activation code will be  used.
[/LIST]
You can download this new version from the Download section of the Code Red LPCXpresso site, at:
http://lpcxpresso.code-red-tech.com/LPCXpresso/Downloads
(login is required)
0 件の賞賛
返信
4 返答(返信)

1,139件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Wed Jul 14 06:13:19 MST 2010
There does seems to be a change of behaviour here which we will investigate.

Couple of things to remember

[LIST]
[*]By default, there is a breakpoint set on main() when you load an image, which means that if your project has 4 other breakpoints set, you actually have 5 breakpoints at load time. You can disable the automatic breakpoint on main, as detailed at

http://lpcxpresso.code-red-tech.com/LPCXpresso/node/48
[/LIST]

[LIST]
[*]You can disable/remove breakpoints from your project before you actually load it via the Breakpoints View (on the tab next to the quickstart panel). So it is probably a good idea to check this before launching a debug session.
[/LIST]
[And remember the 4 breakpoints on LPC11 comes from the Cortex-M0 processor core's debug hardware]

Regards,
CodeRedSupprot
0 件の賞賛
返信

1,139件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by termohlen on Wed Jul 14 04:29:45 MST 2010
Just loaded and started using v3.4 (using with LPCXpresso: LPC1114).  I have found that I can now only use 3 breakpoints and when I forget an use the forth, a lingering process uses > 30% of my cpu. I have to manually kill the process.  :confused:
0 件の賞賛
返信

1,139件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Jul 13 06:44:41 MST 2010
I'm sorry, but there currently no support for Linux. Where does it mention there is support for Red Hat (or any other Linux)?
0 件の賞賛
返信

1,139件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ksinkar on Tue Jul 13 04:08:52 MST 2010
On your downloads page you have mentioned that a LPCXpresso version for Red Hat Linux is there on the CD. Is there any Web link from where I can download the software for Red Hat Linux? I have Fedora 13 on my PC and would love to have the LPCXpresso on that.
0 件の賞賛
返信