LPCXpresso v3.3.4 released

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCXpresso v3.3.4 released

1,071 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Apr 13 10:38:51 MST 2010
We are pleased to announce the release of LPCXpresso v3.3.4.
This release:

[LIST]
[*]Adds support for 64-bit Windows hosts (XP SP2 and greater).
[*]Adds a flash programming utility. Use from a button on the toolbar or  right-click on an executable and select Binary Utilities->Program  Flash
[*]Updated Examples and new Getting Started
[*]Split the "Common" preference into "General" and "Paths and  Directories"
[*]Replaces v3.3.3
[/LIST]
You can download this release from
http://lpcxpresso.code-red-tech.com/LPCXpresso/Downloads
(Login required)
0 Kudos
Reply
4 Replies

1,064 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bigamer on Wed Apr 14 18:08:25 MST 2010

Quote: brucesegal
From the release notes (displayed during install)



Hi [COLOR=#5174a3]brucesegal[/COLOR],

Thanks for your reply.:)
0 Kudos
Reply

1,064 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by brucesegal on Tue Apr 13 23:21:11 MST 2010

Quote: bigamer
I have just updated my lpcxpresso to v3.3.3. What's the difference between v3.3.4 and v3.3.3?:(



From the release notes (displayed during install)


Quote:
LPCXpresso (powered by Code Red Technologies)

Release History
v3.3.4
- Addressed problem which prevents connection to LPC17xx target
- Fixed LPC31xx semihosting wizard
v3.3.3
- added support for 64-bit DFU
- added flash programming utility. Use from a button on the toolbar or right-click on an executable and select Binary Utilities->Program Flash
- updated examples, getting started
- split the "Common" preference into "General" and "Paths and Directores"
- various minor bug fixes and miscellaneous improvements

0 Kudos
Reply

1,064 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bigamer on Tue Apr 13 23:02:48 MST 2010
I have just updated my lpcxpresso to v3.3.3. What's the difference between v3.3.4 and v3.3.3?:(
0 Kudos
Reply

1,064 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Tue Apr 13 19:43:34 MST 2010
Hello CodeRed,

I think it's a good idea to use the post "LPCXpresso Announcements", because the forum already has many users, and within hours  the ad will disappear.

Thank you for this new version, soon we'll be testing

---
Congratulations CodeRedSupport: 300 post!

[COLOR=Red]You've  won a t-shirt with the logo of NXP.
[/COLOR]---[COLOR=Red]
[/COLOR]
0 Kudos
Reply