LPCXpresso licenses

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCXpresso licenses

1,176 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sc_cstjean on Tue Jun 09 08:04:05 MST 2015
This is addressed particulary to the LPC support.

I am a teacher and we plan to use LPCXpresso and LPC1769 board for academic use. I am thinking that the free edition will be sufficient for our needs because the students will create small projects to understand each peripherals in the LPC1769. My problem is that we have to install LPCXpresso on 24 and maybe more PC and we will have to do the process to activate each PC in the lab with the activation code. Is there a mean to activate all PCs in one shut after the image of PCs will be deployed? Or have you other solution to suggest for our needs?

Sylvain Cote
Teacher
Electronic Department
Cegep St-Jean-sur-Richelieu, QC, Canada
0 Kudos
Reply
4 Replies

1,168 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sc_cstjean on Tue Jun 09 18:35:03 MST 2015
Thanks for the information.
0 Kudos
Reply

1,168 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Jun 09 09:06:51 MST 2015
An activation code on a single computer, having been re-imaged with the same OS, should remain the same, but is not guaranteed.

There is no limit to the number of activations made per account.
0 Kudos
Reply

1,168 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sc_cstjean on Tue Jun 09 08:52:26 MST 2015
It is because the PCs can be imaged two or more times in a year. Can we reuse the activation code if the PCs are re-imaged?.
Have we the permission to have many activation codes in a single account if we create one for our institution?

Regards
0 Kudos
Reply

1,168 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Jun 09 08:06:21 MST 2015
Sorry, this is not possible. Each instance of LPCXpresso has to be activated individually.
0 Kudos
Reply