LPCXpresso and open-source debug probe

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCXpresso and open-source debug probe

1,019 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by abonent on Fri Apr 04 05:03:30 MST 2014
Hello,
apart from LPCXpresso boards and LPC Link 2 debug probe, is there any support for other debug probes, like Versaloon or any other open-source probe?
0 Kudos
Reply
3 Replies

1,000 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Apr 04 06:26:19 MST 2014
Off the top of my head, the Peripheral view, and all the Trace stuff will be unavailable. Also, the Registers view will just show the base core registers and not some of the additional registers available through the fully supported probes.
0 Kudos
Reply

1,000 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by abonent on Fri Apr 04 06:03:22 MST 2014
Thank you much, that looks good.
Just curious, what is the advanced debug functionality, unavailable for this operation mode?
0 Kudos
Reply

1,000 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Apr 04 05:36:51 MST 2014
Not directly, but if you have a probe that provides a GDB Server connection, then you can use the same technique as used by Segger J-Link, as described here:
http://www.segger.com/nxp-lpcxpresso.html
(just ignore the J-Link specifics)

Note that when using 3rd party debug probes, some of the advanced LPCXpresso debug functionality will not be available.
0 Kudos
Reply