LPCXpresso: License restriction

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCXpresso: License restriction

734 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by PYI on Thu May 05 03:07:42 MST 2011
I have:
- LPC-Link (NXP);
- LPCXpresso (Code-Red);

Registred on code-red-tech.com - Installed LPCXpresso - Send Serial Number - Enter Activation Code.
LPCXpresso set FULL-version:
License type: FULL
Debug limit: 128k
Activation code: XXXX-XXXX-XXXX-XXXX-XXXX-XXXX-XXXX-XXXX
A FULL copy LPCXpresso may be used for production.

Create Workspace - Setting examples (examples.lpc13xx.new.zip и lpc1343_xpr_bb_101027.zip).
When I download from LPCXpresso Debug-version for axf-files large 8K - message:
Target reported errors.
Reason:
License restriction: flash image too large for this license.
During downloading: view red srting, but clear.

Release-version for axf-files large 8K - download.
LPCXpresso enter in Debuger, but it work with glick.

Uninstalled, Installed - without change.

How does this problem remove?
Best regards, Yura Polomar.
0 Kudos
Reply
1 Reply

700 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu May 05 03:49:13 MST 2011
Did you try:

http://support.code-red-tech.com/CodeRedWiki/LPCXLicenseDiag
0 Kudos
Reply