LPCXpresso LPC11C24 Rev B - USB Driver Problem with Win 7 (64Bit)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCXpresso LPC11C24 Rev B - USB Driver Problem with Win 7 (64Bit)

740 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by user456793 on Tue Jan 12 09:28:15 MST 2016
Hi,

my LPCBoard, LPCXpresso LPC11C24 Rev B, is not booting with the LPC-Link Firmware on my Windows 7 (64 Bit) PC.
I can see the USB Device with DFU Capabilities, when I connect the board.
But when I try to programm it with "bootLPCXpresso.cmd hid" from the script directory, I get the message "Device does not support DFU" or the dfuapp.exe doesn't come to an end, so that I have to kill the dfuapp.exe.
I tried: different USB cable, with and without USB Hub, software version LPCXpresso_6.1.0_164 and LPCXpresso_8.0.0_526, and even a second LPCXpresso board.
What else can I do?

Thanks

Steffen
0 项奖励
回复
1 回复

702 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vtw.433e on Tue Jan 12 09:49:00 MST 2016
Read this FAQ?
https://www.lpcware.com/content/faq/lpcxpresso/booting-lpc-link
0 项奖励
回复