LPCXpresso IDE, project management

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCXpresso IDE, project management

808 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by james on Sun Sep 30 23:59:05 MST 2012
Hi,

I have created a project (version 1), and would like to improve it (version 2) while retaining the old code.

I copy the entire project folder and paste in the project explorer with the name "copy of myproject". But I cannot build this project, it returns a lot of errors such as "undefined referrence to blar blar" I have check that by copying the entire folder, all the project referrences, includes, are also copied. What did I forgot to do?

Just to be safe, I also delete all includes, and re-include all the folders, but it still does not work??

I also created a new project using the "new project" wizard, copy the 'src' folder and relink all the project referrences and includes, and it does have the same error :(

I would be really helpful if someone to point out to me what I have missed.

Thanks()
0 项奖励
回复
2 回复数

796 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by james on Mon Oct 01 02:30:54 MST 2012
Thanks zero, that totally works now
0 项奖励
回复

796 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Mon Oct 01 00:38:41 MST 2012
Check  Library and Library path in your project:

    Properties -> C/C++ Build -> Settings -> Tool Settings -> MCU Linker -> Libraries
0 项奖励
回复