LPCXpresso IDE 5 Released

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCXpresso IDE 5 Released

633 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Fri Nov 09 06:05:22 MST 2012
Today we have released a new version of the LPCXpresso IDE - LPCXpresso 5. This release is available for Windows, Linux and Mac OS X and can be downloaded now, from  http://lpcxpresso.code-red-tech.com/LPCXpresso/Downloads

The LPCXpress 5 IDE is a significant upgrade over previous releases.  The new functionality in LPCXpresso 5 includes: 

[LIST]
[*]The IDE is now based on the Eclipse “Juno” release and CDT 8.1.
[LIST]
[*]The moving to Eclipse “Juno”/CDT 8.1, provides a number of interesting enhancements to the Code Red IDE version 5, including:
[LIST]
[*]New look to workbench
[*]Ability to mix views and editors
[*]A universal search bar
[*]Ability to detach editors
[*]Global build console
[/LIST]

[*]The following links provide more details of some of the improvements at the general IDE level:
[LIST]
[*]Whats new in Juno
[*]Whats new in CDT
[/LIST]

[/LIST]

[*]The compilation tools are now based on GCC 4.6.2.
[LIST]
[*]New in GCC 4.6.2
[/LIST]

[*]Red Trace enhancements
[LIST]
[*]Support for Instruction Trace for Cortex-M3/M4 based MCUs implementing an Embedded Trace Buffer (ETB).
[*]Support for Instruction trace for Cortex-M0+ based systems implementing a Micro Trace Buffer (MTB).
[/LIST]

[*]Updated Redlib C library
[LIST]
[*]Cortex-M4 specific library variants now provided, rather than just  relying on Cortex-M3 variant. Should lead to some performance  improvements, particularly when (single precision) floating point is  being used.
[*]`printf` family functions no longer pull in `ctype` constant data,  saving ~400 bytes of flash space for applications using any of these  functions.
[/LIST]

[*]Red State enhanced
[LIST]
[*]Support for multiple state machines in a single project
[/LIST]

[*]Additional Debug probe support
[LIST]
[*]Support for direct debug connection to Code Red's RDB4078 board.
[/LIST]

[/LIST]
0 项奖励
回复
0 回复数