LPCXpresso Better every day

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso Better every day

554件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Wed Jun 29 15:46:51 MST 2011
Hello CodeRed,

My first test for LPCXpresso 4.x (Mandriva Linux) showed very good results, now also works "Program Flash".

Some small things go wrong here:
- "Target selection for null"

Should be selected by default the microcontroller being used.

- "Reset target on completion"

Always produces the same output:
"Nt: Connected: was_reset=false. was_stopped=true"

The command line is always the same:
crt_emu_lpc11_13_nxp -g -2 -pLPC1111/101 -flash-load-partial="/home/xxx/workspace/LPCXpresso1114_blinky/Release/LPCXpresso1114_blinky.axf" -wire=winUSB  -s250


- I have an old version installed, and the "Start menu" shows the same label, should say "LPCXpresso 4.x" to avoid confusing versions.

Thank you.
0 件の賞賛
返信
0 返答(返信)