LPCXpresso 7.8 hungs on debug

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCXpresso 7.8 hungs on debug

1,306 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by elgarbe on Thu Jul 09 09:59:06 MST 2015
Hi, I'm using LPCXpresso 6.1.4 without problem on my XP SP2 machine and LPCLink from LPC1769 evaluation board.
Now I install 7.8. I can compile my old projects, but when I try to debug it hangs. I see Lunching Term_Temp 39% on status bar but the ide is hung (mouse is sand clock). I don't know where the log file is to attached.

Thank
0 Kudos
Reply
5 Replies

1,298 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by elgarbe on Mon Jul 13 16:00:50 MST 2015
LPCXpresso v7.5.0_254 works ok on XP SP3. don't work on XP SP2
7.8 don't work on XP SP3

regards
0 Kudos
Reply

1,298 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by elgarbe on Thu Jul 09 11:23:30 MST 2015
The problemas is that lpcxpresso ide hungs and stop working. I have to go to process administrator and terminate lpcxpresso proces.
I will try disabling other probes.
I have another pc with xp and lpcxpresso 7.5 works fine, I don't remember if it's a sp2 or sp3
Thank
0 Kudos
Reply

1,298 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by whitecoe on Thu Jul 09 11:14:24 MST 2015
You don't actually tell us what the actual error you get is, but as you are using LPC-Link, you could try disabling other probes - just in case one of them is causing the problem, as described in http://www.lpcware.com/content/forum/connect-timed-out

HTH!
0 Kudos
Reply

1,298 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Jul 09 10:33:06 MST 2015
As stated in the release notes Windows XP is not supported. We stopped supporting XP when Micosoft stopped supporting it. Sorry.
0 Kudos
Reply

1,298 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by elgarbe on Thu Jul 09 10:02:36 MST 2015
same problem with 7.7.2 and 7.5.0

thank!
0 Kudos
Reply