LPC812-LPC link-2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC812-LPC link-2

2,472件の閲覧回数
abhishektiwari
Contributor I

I am working with a custom board with LPC812. I am getting following issues while connecting it with LPCexpresso:

1- In the debugger option it is showing only SWD mode not JTAG.

2- I am not able to connect in SWD mode. Error is " cannot connect to core"

plz. suggest a solution.

0 件の賞賛
返信
3 返答(返信)

2,036件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

There's a power problem, or there's something wrong with your debug circuit. Pay attention to the debug circuit design recommentations, and sharing GND.

Thanks and regards,

LPCXpresso Support

0 件の賞賛
返信

2,036件の閲覧回数
converse
Senior Contributor V

1. The is no JTAG debug on LPC812 it is SWD only for debug

2. Check your debug circuit: https://community.nxp.com/message/630601 

0 件の賞賛
返信

2,036件の閲覧回数
abhishektiwari
Contributor I

I have connected SWDIO,SWCLK and GND from LPC-Link-2 board to my custom board as suggested, Still same error.

plz. suggest.

0 件の賞賛
返信