LPC812 IAP Write FLASH

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC812 IAP Write FLASH

933 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mvinger on Sat Jun 22 21:58:23 MST 2013
Anyone out there used a 64-byte page as a pseudo-eeprom?
I have read the docs and was wondering if anyone had any pointers to jumpstart my storing of parameters in the FLASH.
I have already allocated the page for my parameters and now just need to write the code using the IAP writing commands but it looks a bit 'hairier' than I was hoping.

Thanks.
MTV2
0 Kudos
Reply
1 Reply

797 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jdesbonnet on Wed Feb 18 12:57:30 MST 2015
Yes, I've got some demo code (for LPC812, but should work with all LPC8xx devices) and some documentation on this:
http://jdesbonnet.blogspot.ie/2015/02/nxp-lpc8xx-eeprom-emulation.html
0 Kudos
Reply