LPC4330 Internet radio demo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4330 Internet radio demo

217 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by srinidhi M on Fri Apr 18 01:51:52 MST 2014
Hello friends,

Am trying to run internet radio demo on lpc4330, when ever i am playing mp3 from SD card am getting song with noise and single frame is playing two three times... If any body worked on it please suggest me.

I will be waiting for the replay.

Thank you
Srinidhi
0 Kudos
Reply
1 Reply

203 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bavarian on Thu Apr 24 08:20:03 MST 2014
As there is no implementation of the internet radio on the LPC4330 I have no idea which board / software / decoder etc you use to run this.
Examples showing how to access an SD card are part of the LPCOpen package.

I assume that you don't have enough performance for the MP3 decoder when you execute from flash, so you need to relocate relevant parts of the decoder into internal SRAm to sped up the decoder execution.

Regards,
NXP Support Team

0 Kudos
Reply