LPC4330 Internet radio demo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4330 Internet radio demo

209件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by srinidhi M on Fri Apr 18 01:51:52 MST 2014
Hello friends,

Am trying to run internet radio demo on lpc4330, when ever i am playing mp3 from SD card am getting song with noise and single frame is playing two three times... If any body worked on it please suggest me.

I will be waiting for the replay.

Thank you
Srinidhi
0 件の賞賛
返信
1 返信

195件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bavarian on Thu Apr 24 08:20:03 MST 2014
As there is no implementation of the internet radio on the LPC4330 I have no idea which board / software / decoder etc you use to run this.
Examples showing how to access an SD card are part of the LPCOpen package.

I assume that you don't have enough performance for the MP3 decoder when you execute from flash, so you need to relocate relevant parts of the decoder into internal SRAm to sped up the decoder execution.

Regards,
NXP Support Team

0 件の賞賛
返信