LPC3154 on lpc-link getting hot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC3154 on lpc-link getting hot

1,371 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by paksoft on Mon Mar 28 09:14:14 MST 2011
Hello dude,
    I have a lpcxpresso LPC1769 ver. B. Just bought it:) And doing some debugging then I noticed the LPC3154 is getting hot while I debugging some code. And I also notice that it will become normal when I quit lpcxpress IDE. LPC1769 on target board is still cool. My question is it's normal?

regards,
pak
0 Kudos
Reply
5 Replies

1,284 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by paksoft on Tue Mar 29 07:01:23 MST 2011

Quote:
FYI - the LPC3154 is supplying power to the LPC1769 via its built-in PSU. So, I would guess you are feeling the heat from the PSU and not from the core itself.



Thanks, TheFallGuy. You've explained my question perfectly. :D

BTW, what is max current drain of VIO_3V3?
Regards,
pak
0 Kudos
Reply

1,284 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Tue Mar 29 02:22:03 MST 2011
FYI - the LPC3154 is supplying power to the LPC1769 via its built-in PSU. So, I would guess you are feeling the heat from the PSU and not from the core itself.
0 Kudos
Reply

1,284 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by paksoft on Tue Mar 29 02:10:02 MST 2011

Quote:
Can you measure the temperature of the LPC3154?



The temperature difference can be compared by touching LPC1769 and LPC3154. I think temprature is about 40 deg C. Have you tried it before? :)

Regards,
Pak
0 Kudos
Reply

1,284 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by larryvc on Mon Mar 28 13:31:11 MST 2011
I just tested mine and the LPC3154 barely gets warm.  I've never noticed it getting hot.

What are you debugging when it gets hot?  Maybe I can duplicate it.

Can you measure the temperature of the LPC3154?
0 Kudos
Reply

1,284 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Mon Mar 28 10:14:14 MST 2011
Yes dude. :)
0 Kudos
Reply